Flow Meter Input Type

The fields on the Meter Input tab vary depending on the Meter Input Type that you selected. This topic describes the fields related to either the Mass flow or Volume flow Meter Input Type. (The latter type of meter input only applies to Liquid and Water Flow Runs.)

You can configure these properties directly in ClearSCADA, or read the configuration into the ClearSCADA database (see Configure or Read the Flow Run Configuration).

The input alarms fields allow you to set the alarm thresholds for alarm types that have been enabled in the Input Properties section.

Use the following to configure alarm limits:

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

ClearSCADA 2017 R2