Using a Script to Create a Form

A common requirement for scripts is to create a Form that is displayed when a Mimic item is selected.

Example:

In this example, we will describe the script that creates the following Form:

The Form contains a Yes/No combo box, a text entry field, and OK and Cancel buttons. The text entry field is for a password, so the entry has to match the specified password. This type of Form could be used to shutdown equipment and so on.

By examining the script that is used to create the Verify Control Action Form, you can learn how to add fields, buttons, and combo boxes to Forms. The script for the Form is:

Option Explicit

 

Public Function VerifyControl(Point)

 

Dim frmComboBox

Dim frmEditBox

Dim frmOKButton

Dim frmCancelButton

 

Dim sMasterPassword

Dim iReturnValue

Dim oClearSCADAPoint

 

sMasterPassword = "abc"

 

Form.Init "Verify Control Action"

Form.AddGroupBox 0,0,100,8,""

 

Form.AddStaticText 2,1, "Are you sure you wish to execute this control?"

Form.AddStaticText 2,3, "Enter master password"

 

Set frmComboBox = Form.AddComboBox(60,1)

frmComboBox.Add("Yes")

frmComboBox.Add("No")

frmComboBox.Selection = 1 '0 is first element, 1 is second, etc.

Set frmEditBox = Form.AddEditBox(60,3)

frmEditBox.Password = True

frmEditBox.MaxLength = 10

frmEditBox.Value = ""

Set frmOKButton = Form.AddPushButton(60,5,"OK")

frmOKButton.Default = True

Set frmCancelButton = Form.AddPushButton(75,5,"Cancel")

 

Form.Show

If Form.Selection = "OK" Then

If frmComboBox.Selection <> 0 Then

iReturnValue = MsgBox("Select ""Yes"" from the pulldown menu for this action to be executed", vbOKOnly+vbExclamation, "Action not executed")

ElseIf frmEditBox.Value <> sMasterPassword Then

iReturnValue = MsgBox("Incorrect password specified", vbOKOnly+vbExclamation, "Action not executed")

Else

Set oClearSCADAPoint = Server.FindObject(Point)

If oClearSCADAPoint Is Nothing Then

iReturnValue = MsgBox("Unable to find the object", vbOKOnly+vbExclamation, "Action not executed")

Else

oClearSCADAPoint.Interface.Override oClearSCADAPoint.Interface.CurrentValue+5

iReturnValue = MsgBox("Action successfully performed",vbOKOnly+vbInformation, "Action performed successfully ")

End If

End If

ElseIf Form.Selection = "" Then'This is when they click Esc or the X, allows them to get some feedback.

'We don't give feedback when they click Cancel

iReturnValue = MsgBox("Action canceled", vbOKOnly+vbInformation, "Action not executed")

End If

End Function

We will now explain each section of the script so that you can understand how the script provides the various features of the Form. You can then use the same scripting principles to create your own Forms.

The script begins with Option Explicit which means the script has to define each function before it uses the functions. The name of the script function is defined as VerifyControl and (Point) defines the variable that represents the FullName value that is entered on the Pick Action Wizard (to define which database item is to be controlled).

Option Explicit

Public Function VerifyControl(Point)

The variables that are used by the script are defined next to Dim entries. The frm is used as the prefix for Form variables, s is the prefix for the string variable, i is the prefix for an integer variable, and o is the prefix for a database item definition. These prefixes are not compulsory, but they are useful as they allow engineers to determine the type of each variable without having to investigate.

Dim frmComboBox

Dim frmEditBox

Dim frmOKButton

Dim frmCancelButton

 

Dim sMasterPassword

Dim iReturnValue

Dim oClearSCADAPoint

The sMasterPassword = "abc" line defines the sMasterPassword variable as being "abc". This means that the user has to enter abc as the password.

sMasterPassword = "abc"

The settings that define the appearance of the Verify Control Action Form are defined by the following lines:

Form.Init "Verify Control Action"

Form.AddGroupBox 0,0,100,8,""

 

Form.AddStaticText 2,1, "Are you sure you wish to execute this control?"

Form.AddStaticText 2,3, "Enter master password"

 

Set frmComboBox = Form.AddComboBox(60,1)

frmComboBox.Add("Yes")

frmComboBox.Add("No")

frmComboBox.Selection = 1 '0 is first element, 1 is second, etc.

The Form.Init "Verify Control Action" sets the title of the Form. The Form.AddGroupBox 0,0,100,8, "" line defines the appearance and position of the section border that is shown within the Form. The coordinates start at the top-left corner and end at the bottom right-hand corner.

The Form.AddStaticText entries define the position and text for the text labels that appear on the Form.

Set frmComboBox = Form.AddComboBox(60,1)

frmComboBox.Add("Yes")

frmComboBox.Add("No")

frmComboBox.Selection = 1 '0 is first element, 1 is second, etc.

 

The Set frmComboBox = Form.AddComboBox (60,1) line defines the location of a combo box on the Form.

The frmComboBox.Add lines define the options that are available in the combo box.

The frmComboBox.Selection = 1 '0 is first element, 1 is second, etc. line sets the numbers for the combo box options. 0 is the first option, 1 is the second option. The text after the ' is commented out.

The following script is used to define the settings for the password field:

Set frmEditBox = Form.AddEditBox(60,3)

frmEditBox.Password = True

frmEditBox.MaxLength = 10

frmEditBox.Value = ""

 

The Form.AddEditBox (60,3) section defines that the field is a text entry field (edit box) and has the coordinates 60, 3. (The coordinates define the field's position on the box).

The frmEditBox.Password = True line sets the password field to hide the text entry and replace the characters with asterisks. This means that the password cannot be seen by other users when an engineer types in the password.

The frmEditBox.MaxLength = 10 line sets the password length to 10 characters.

The frmEditBox.Value = "" line sets the password field to be empty by default.

The following script is used to define the OK and Cancel buttons:

Set frmOKButton = Form.AddPushButton(60,5,"OK")

frmOKButton.Default = True

 

Set frmCancelButton = Form.AddPushButton(75,5,"Cancel")

The OK button is set to be highlighted by default (= True), so that if the user presses the Enter key, the OK button is selected.

If the user selects the OK button on the Form, ClearSCADA checks to see if the Yes option has been selected in the combo box. If it has not been selected, a dialog box is displayed. The message box displays the message 'Select "Yes" from the pulldown menu for this action to be executed'. The title of the dialog box is "Action not executed". This is defined by the following section of the script:

Form.Show

If Form.Selection = "OK" Then

If frmComboBox.Selection <> 0 Then

iReturnValue = MsgBox("Select ""Yes"" from the pulldown menu for this action to be executed", vbOKOnly+vbExclamation, "Action not executed")

If the user selects the OK button on the Form and the Yes option has been selected, ClearSCADA checks to see if the correct password has also been entered.

If the incorrect password has been entered, a dialog box is displayed containing the message "Incorrect password specified". The title of the dialog box is "Action not executed".

This is defined by the following section of the script:

ElseIf frmEditBox.Value <> sMasterPassword Then

iReturnValue = MsgBox("Incorrect password specified", vbOKOnly+vbExclamation, "Action not executed")

If the correct password is entered, but ClearSCADA cannot locate the database item, a dialog box is displayed. The dialog box contains the message "Unable to find the object". The title of the dialog box is "Action not executed".

This is defined by the following section of the script:

Else

Set oClearSCADAPoint = Server.FindObject(Point)

If oClearSCADAPoint Is Nothing Then

iReturnValue = MsgBox("Unable to find the object", vbOKOnly+vbExclamation, "Action not executed")

 

If the correct password has been entered, ClearSCADA attempts to locate the database item that is represented by the Point variable. The point that this variable represents is selected on the Pick Action Wizard when the script is set up as the Mimic item's pick action. The Pick Action Wizard has to be set to reference a FullName property of an object or another property that contains the fullname of the object. In this case, we will assume that the Pick Action Wizard is set to reference the FullName property of the point.

If the database item can be found, an Override method is performed and sets the value to 5. When the override has taken place, a dialog box is displayed containing the message "Action performed successfully".

This is defined by the following section of the script:

Else

oClearSCADAPoint.Interface.Override oClearSCADAPoint.Interface.CurrentValue+5

iReturnValue = MsgBox("Action successfully performed",vbOKOnly+vbInformation, "Action performed successfully ")

End If

If the user selects the Close window button (at the top corner of the Form) or presses the Esc key, the action is canceled. A dialog box is displayed containing the message "Action canceled", and it has the title "Action not executed". There is no dialog box message if the user selects the Cancel button.

This is defined by the following section of the script:

ElseIf Form.Selection = "" Then'This is when they click Esc or the X, allows them to get some feedback.

'We don't give feedback when they click Cancel

iReturnValue = MsgBox("Action canceled", vbOKOnly+vbInformation, "Action not executed")

End If


Disclaimer

ClearSCADA 2017 R2