Hardware and Operating System Security
The security of ClearSCADA is also dependent on the operating system as well as the hardware platform on which it is installed. The following sections are aimed at System Administrators who are setting up and configuring the systems prior to the installation of ClearSCADA and are recommendations that should be considered to improve the general security.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.