About the Tutorial

The ClearSCADA tutorial is designed to help first-time or inexperienced ClearSCADA users get used to working in ViewX and WebX (the two main ClearSCADA user interfaces). Each section of the tutorial contains easy-to-follow instructions with explanations of the effects of your actions. As you work through the tutorial, you will learn about the common configuration procedures, displays, and methods used for accessing features.

Although each section includes instructions and helpful information, the tutorial is only designed to be a guide to ClearSCADA and is not a substitute for the comprehensive online help documentation or a training course. Also, while the tutorial is aimed at first-time users, we recommend that users have a strong background in both programmable logic controllers (PLCs) and personal computers using Windows.

Throughout the tutorial, we have used the following conventions:

We recommend that you complete each of the tutorial sections in order, but if you wish to skip certain sections, you can do this. However, you may need to import files relating to the sections you have skipped. Instructions on how to import the files are included at the start of the sections.

Finally, if you are working on the tutorial and your system stops running, you will need to restart your server. This is because demo ClearSCADA systems are set to stop running after 2 hours. For information on restarting the ClearSCADA server, see Restarting your System.

If you are ready to start the tutorial, proceed to Using the ViewX Interface.


Disclaimer

ClearSCADA 2017 R2