WITS-Specific Alarm and Event Categories

Each alarm and event in a ClearSCADA system has a Category that indicates the type of alarm or event. The Category is included by default in the Events List and, if applicable, in the Alarms List and in the Alarm Banner.

You can optionally filter the entries in either List by category—the entries from which you can choose comprise various ‘core’ categories, along with any categories that are specific to the drivers that are installed on your system.

In systems in which both the DNP3 and DNP3 WITS driver components are installed, in addition to the ‘core’ and DNP3 driver-specific alarm and event categories, there is a DNP3 WITS-specific category as follows:

 

Further Information

DNP3 Specific Alarm and Events Categories: see DNP3 Specific Alarm and Event Categories.

Events Lists and ‘core’ filter categories: see the ClearSCADA Guide to Lists.

Alarms Lists and ‘core’ filter categories: see the ClearSCADA Guide to Alarms.


Disclaimer

ClearSCADA 2017 R2