Welcome to the Guide to the Database

Document Scope

The ClearSCADA Guide to the Database provides information about the structure of the ClearSCADA database. It also explains how to use the ClearSCADA Database Schema to locate specific information about the database tables.You may need to access this information when:

Intended Audience

This guide is designed to help users understand the structure of the ClearSCADA database. The information it contains may be useful to engineers who are responsible for configuring:

This guide also provides information about the Configuration Change CRC feature that can be used to help to detect whether an item's configuration has changed (see Understand Configuration Change CRCs).

If you are unfamiliar with the structure of the database and how the ClearSCADA Database Schema works, we suggest that you:

  1. Familiarize yourself with the structure of the database (see Understanding the Database).
  2. Learn how to use the ClearSCADA Database Schema to view information about different tables (see Working with the Database Schema).

Disclaimer

ClearSCADA 2017 R2