Configure the Scanner Properties

Use the fields on the Scanner tab to define the driver-specific properties of a scanner. Some of these fields are common to many scanners (see Configuring Scanners on Simple Drivers in the ClearSCADA Guide to Simple Drivers). Those fields that are specific to scanners on the EWS Client Driver are described below.

For more information about setting scan rates and offsets see Define the Scan Rate in thee Simple Drivers Guide.


Disclaimer

ClearSCADA 2017 R2