Disable Indexing on C drive

We recommend that the use of the built-in disk indexing service within Windows is disabled for all connected drives as this impacts on the system performance, in particular for Virtual Environments.

The performance of drives that are allocated for the storage of events or historic data, where they are under constant change with the addition of files would be severely impacted as a result of the indexing service constantly re-applying updates to its internal reference database.


Disclaimer

ClearSCADA 2017 R2