Promote

The Promote permission defines whether the user or User Group can promote an outstation, PLC etc. so that is scanned in preference to other devices. This is dependent on the configuration and the supported features of the outstation or PLC.

To promote a device, you need access to the Promote Scanning action.

The Promote permission also provides access to the Promote Dial Out action.

Availability: Can be restricted via the Permission Restrictions settings (see Define whether any Permissions are Restricted).


Disclaimer

ClearSCADA 2017 R2