De-Militarized Zone (DMZ) Permanent Standby Servers

De-Militarized Zone (DMZ) Permanent Standby servers are servers that are used as an additional part of a Hot-Standby Pair or Triple Standby architecture. Like 'normal' Permanent Standby servers, they can only be set to Standby and cannot switch to Main. However, they have one key difference to 'normal' Permanent Standby servers—DMZ servers have no connection back to the system, and so cannot write to the system. This means that DMZ Permanent Standby servers offer more protection against malicious attacks, as they cannot be used to write data or interfere with the ClearSCADA database. Another benefit is that as there is no connection back to the system, it makes the configuration of a firewall between the system and the DMZ Permanent Standby server a much simpler task.

As DMZ Permanent Standby servers are unable to write to the ClearSCADA database, they cannot be used to change passwords. If a user’s password expires, they will need to define a new password on a non-DMZ server.

If the DMZ Permanent Standby server uses an Active Directory connection, then it can be used to change passwords that are also used within ClearSCADA. However, users cannot be created automatically by logging on to a DMZ Permanent Standby with an Active Directory connection.

DMZ Permanent Standby servers are only able to provide read-only access to clients. Any clients that connect to ClearSCADA via a DMZ Permanent Standby server can be used to display data, but cannot be used to perform controls etc.

With a 'normal' Permanent Standby server, the Permanent Standby server can send data to, and receive data from the Main and Standby servers.

With a DMZ Permanent Standby server, the DMZ Permanent Standby server can only receive updates from the Main server (as part of the synchronization process). Any read requests are handled locally by the DMZ server itself, based on the information it has received from the Main server.

As with normal Permanent Standby servers, DMZ Permanent Standby servers can be used:

ClearSCADA allows you to connect up to four DMZ Permanent Standby servers to a Hot Standby Pair architecture or up to three DMZ Permanent Standby servers to a Triple Standby architecture. Typically, a system that uses DMZ Permanent Standby servers is set up as follows:

To set up a multi-server architecture that uses one or more DMZ Permanent Standby servers, refer to the following section:


Disclaimer

ClearSCADA 2017 R2