Requirements for Citrix XenApp or Microsoft Remote Desktop Services

(Microsoft Remote Desktop Services was formerly known as Microsoft Terminal Services.)

To use ClearSCADA with Citrix XenApp or Microsoft Remote Desktop Services effectively, you should check that the:

In the following sections, we provide information on the system specifications needed to run ClearSCADA on Citrix and Remote Desktop Services:

For more details on the specifications for Citrix XenApp and Microsoft Remote Desktop Services, please contact the agent or vendor.


Disclaimer

ClearSCADA 2017 R2