Server Command Line Tool

You can use the built-in ClearSCADA Server Command Line Tool to run commands from the Windows command prompt. This can be useful if you need to access the ClearSCADA server commands from other programs or via remote access that limits you to using command lines. For example, you may want to run ClearSCADA server commands within batch files for third-party software applications.

In this section, we explain how to:


Disclaimer

ClearSCADA 2017 R2