Configure the General Generic Modbus Analog Point Properties

NOTE:This section provides information about ‘Generic’ analog points. If your system is running an Advanced Modbus Extension Driver, other types of Advanced Modbus analog point might be available. For information about non-generic Advanced Modbus analog points, see the relevant Advanced Modbus extension driver guide.

Use the fields at the top of the Analog Point tab on the Generic Modbus Analog Point Form to Configure Common Point Properties. Fields that are specific to Generic Modbus Analog points are explained below.


Disclaimer

ClearSCADA 2017 R3