Define a Counter-Type Point’s Trend Settings

You can display the trend, or movement, of a counter-type point’s value in the form of a graph. The graph is referred to as a Trend. Up to two types of Trend are available per point, depending on the point configuration (see Types of Trend).

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3