DNP3

Already Executing Alarm

Associated with: DNP3 master outstations

The Already Executing Alarm attribute indicates whether the outstation’s DNP3 ALREADY_EXECUTING IIN bit is set.

If the bit is set, this indicates that there is a problem executing one of the following functions:

Possible states: Displays one of the Standard Alarm States.

If the ALREADY_EXECUTING IIN bit is set, use the outstation’s diagnostic features to determine why the outstation could not execute the function. For example, it could be that the outstation was unable to execute an action sent from ClearSCADA because at that time, the outstation was already executing the action as part of an internal logic program. When you have discovered why the outstation could not execute the function, you will need to determine whether there is a problem at the outstation or if it is just a case that the outstation was busy when ClearSCADA sent the request.


Disclaimer

ClearSCADA 2017 R3