DNP3

Data Processing Alarm

Associated with: DNP3 master outstations

The Data Processing Alarm attribute indicates whether the SCADA master (ClearSCADA) has been unable to process a data response from the outstation. The master is unable, for example, to process data that is formatted incorrectly or that includes unsupported content.

Possible states: Displays one of the Standard Alarm States.

See the outstation documentation for information on clearing the Data Processing IIN bit.


Disclaimer

ClearSCADA 2017 R3