DNP3

Define the PSTN Idle Timeout

Use the PSTN Idle Comms Timeout field on the PSTN tab to specify the maximum amount of time that a Slave maintains PSTN communications with its master when no communications traffic is detected on the line that is in use.

If no further communications traffic is detected, the call is terminated once the timeout elapses.

Specify the required timeout period in seconds.


Disclaimer

ClearSCADA 2017 R3