DNP3

Disable Unsolicited Alarm

Associated with: DNP3 master outstations

The Disable Unsolicited Alarm attribute indicates whether the DNP3 ‘Disable Unsolicited’ message, sent by the ClearSCADA DNP3 driver to disable unsolicited responses in the outstation, was successful.

The ClearSCADA DNP3 driver will send the ‘Disable Unsolicited’ message if:

Possible states: Displays one of the Standard Alarm States.

Use the Unsolicited Event Reporting Status >attribute to determine which unsolicited event classes are enabled and disabled in the outstation.


Disclaimer

ClearSCADA 2017 R3