DNP3

Event Buffer Overflow Alarm

Associated with: DNP3 master outstations

The Event Buffer Overflow Alarm attribute indicates whether the outstation’s DNP3 EVENT_BUFFER_OVERFLOW IIN bit is set. This bit is set by the outstation when it has to discard events due to its internal event buffer being full. This might occur when an outstation has been offline for an extended period of time, or it is logging events too quickly and therefore its buffers are filling more quickly than expected. (Which events an outstation discards is outstation-specific. Some outstations might discard the oldest events, whereas other outstations might discard the newest events. Refer to a device’s DNP3 Profile document to determine which events it will discard.)

Having an outstation report that its EVENT_BUFFER_OVERFLOW IIN bit is set is a serious condition as it means data has been (and is still being) lost, so it is vital that the cause of the event buffer overflow is rectified as soon as possible. The problem might be due, for example, to bad configuration, a bad sensor, or communication problems. Once the problem is rectified and healthy communications are re-established, ClearSCADA will upload events from the outstation until all events have been successfully uploaded.

Possible states: Displays one of the Standard Alarm States.

If the event buffer of the outstation overflows regularly, do one (or more) of the following:


Disclaimer

ClearSCADA 2017 R3