DNP3

Freeze and Clear

Associated with: DNP3 master outstations that support Frozen Counter points

Security permission required to access this pick action: Diagnostics

Use the outstation’s Freeze and Clear pick action to copy the values of the Counter Points to their associated Frozen Counter Points, and then reset the Counters back to a pre-configured value. The reset value is determined by the Slave and is typically zero.

The pick action takes into account the Freeze settings configured on the Outstation Form (see Configure Frozen Counter Support).

Also see Freeze.

If using this pick action with the Automation Interface, you need to specify the method name FreezeClear.


Disclaimer

ClearSCADA 2017 R3