DNP3

Read String

Associated with: DNP3 String Points

Security permission required to access this pick action: Diagnostics

Use the Read String pick action to update the value of the string point in the ClearSCADA database.

If using this pick action with the Automation Interface, you need to specify the method name RequestRead.


Disclaimer

ClearSCADA 2017 R3