DNP3

Significant Change Properties

Use the fields within the Significant Change section of the Analog Point tab to specify when ClearSCADA updates its database with the value reported by the outstation. For further information, see Define the Criteria for a Significant Change in Value in the ClearSCADA Guide to Core Point Configuration.


Disclaimer

ClearSCADA 2017 R3