DNP3

Specify the Outstation from which ClearSCADA is to Retrieve Status Data

Use the Outstation field on the Parent tab to specify the DNP3 outstation that ClearSCADA is to scan for status data:

Use the field’s browse button to display a Reference browse window and select the required outstation entry from the window.


Disclaimer

ClearSCADA 2017 R3