Configure General Ethernet Properties

SCADAPack E outstations are supplied with 1, 2 or 3 Ethernet interfaces. Use the fields within the Ethernet 1 and, if applicable, the Ethernet 2 and Ethernet 3 sections of the SCADAPack TCP/IP tab to define the general properties for the interface(s).

If the outstation does not have the Ethernet 2 and Ethernet 3 interfaces, the fields within those sections of the tab are ‘grayed out’ and unavailable for use. This is defined by the Outstation Type property (see Specify the Outstation Type).


Disclaimer

ClearSCADA 2017 R3