Configure Rate of Change Properties

Use the fields within the Rate of Change section of the Analog Point tab to define if the SCADAPack E outstation detects whether a DNP3 SCADAPack point’s value is rising or falling too quickly.

Rate of Change properties do not apply to analog points for which the Point Type is set to Physical Output (see Configure Common Properties of DNP3 SCADAPack Points).

A DNP3 SCADAPack Binary Input Point that is linked to one Rising Point or Falling Point cannot be linked to any other Rising Point, Falling Point, No Change Point (see Specify Whether the SCADAPack Outstation is to Detect if an Analog Point has Stopped Changing), control Interlock Point (see Interlock Points), or I/O Status Point (see Configure the 5000 Series I/O Properties).


Disclaimer

ClearSCADA 2017 R3