Configure the Event Deviation Properties

Use the fields within the Event Deviation section of the Analog Point tab to determine the circumstances in which a SCADAPack E outstation should generate an event for a DNP3 SCADAPack point, based on a change in the point’s value.

With physical analog inputs, you can use the Event Deviation properties to help prevent the SCADAPack E outstation from reporting insignificant fluctuations in value to ClearSCADA. This can help reduce the bandwidth usage between ClearSCADA and the outstation, and improve performance of historical data access (for example, Trends).


Disclaimer

ClearSCADA 2017 R3