Configure the Security Configuration Properties

This section only applies to outstations on which DNP3 Secure Authentication is enabled.

With a DNP3 outstation that is to communicate using DNP3 Secure Authentication, you need to enable security and configure the properties on the outstation’s Security tab (see Configure the Security Properties in the ClearSCADA Guide to the DNP3 Driver). The settings on the Security tab are used by ClearSCADA to determine the outstation’s security settings. They also determine how ClearSCADA interacts with that outstation with regard to security—the settings are not downloaded to the actual outstation.

With SCADAPack E outstations, you can also configure the actual outstation’s security settings remotely, then download those settings to the outstation. To do this via ClearSCADA, you need to import the security configuration file into ClearSCADA, associate that file with the relevant outstation, then download that file to the outstation (see Import and Download SCADAPack Security Configuration Files). You use the fields in the Security Configuration section of the Outstation Form’s SCADAPack tab to associate the relevant security configuration file with an outstation. In order to configure the Security Configuration properties successfully, a suitable DNP3 SCADAPack Security Configuration item has to exist in the ClearSCADA database (see Import and Download SCADAPack Security Configuration Files).


Disclaimer

ClearSCADA 2017 R3