File

Associated with: DNP3 SCADAPack Firmware Image items.

This status attribute indicates the name of the compressed binary firmware image file that was last imported into the ClearSCADA database using this particular DNP3 SCADAPack Firmware Image item (see Import Firmware Image). The date and time of the last import process is included.

Use this status attribute in conjunction with the Description attribute to ascertain information about the .biz file with which this particular DNP3 SCADAPack Firmware Image item is associated.

Example:

"\750e386.biz" Modified at Mar/15/2007 15:37:24.000


Disclaimer

ClearSCADA 2017 R3