General Properties

Use the fields at the top of the Analog Point tab to define the general properties of a DNP3 SCADAPack Analog point.

For further information on these properties, see Configure Common Properties of DNP3 SCADAPack Points in this guide, and see Configure General Point Properties in the ClearSCADA Guide to the DNP3 Driver.


Disclaimer

ClearSCADA 2017 R3