SetVectors

Associated with: DNP3 SCADAPack Analog Profiles, DNP3 SCADAPack Binary Profiles, and DNP3 SCADAPack Counter Profiles

Security permission required to access this method: Configure

Use the SetVectors method to define all of the profile vectors on a DNP3 SCADAPack Profile item that exists in the ClearSCADA database.

The method is the equivalent of manually editing a profile’s vectors in ViewX (see Configuring DNP3 SCADAPack Profiles).

The SetVectors method arguments vary, depending on the type of Profile. For more information, see:

With each type of Profile, the arguments comprises a Times and one or more <Value Type>Values arrays. Ideally the <Value Type>Values arrays should contain the type of value that corresponds to the Profile’s type (for instance floating point 32-bit values to configure a DNP3 SCADAPack Analog Profile’s vectors). However, if an array contains different type(s) of value, ClearSCADA will automatically convert those values to the correct type when the SetVectors method is executed.

To successfully configure a DNP3 SCADAPack Profile’s vectors using the SetVectors method, you need to ensure that:

If any of the above requirements are not adhered to, the method call will not succeed and ClearSCADA will not modify the DNP3 SCADAPack Profile’s vectors.


Disclaimer

ClearSCADA 2017 R3