Specify how the SCADAPack Outstation Handles Underrange, Overrange and Invalid RTU Events

The Out of Range RTU Event field is displayed at the bottom of the Alarm Limits section on the Analog Point tab:

If the Area of Interest feature is enabled on your system, an Area of Interest field is displayed below the Out of Range RTU Event field. For information on this property, see Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events.


Disclaimer

ClearSCADA 2017 R3