Tune Limits Alarm

Associated with: DNP3 SCADAPack Analog points and DNP3 SCADAPack Counter points.

This status attribute indicates an alarm state if ClearSCADA’s last attempt to download the point’s alarm limits configuration to the SCADAPack E outstation was unsuccessful. ClearSCADA attempts to download such configuration in response to a Tune Alarm Limits pick action request.

For example, a download would be unsuccessful if communications were lost during the download, or an attempt was made to tune the limits of a point for which configuration did not yet exist in the outstation.

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R3