UpdateFileProperties

Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations

Security permission required to access this method: Configure

Use this method to update the property parameters for a file that exists in a DNP3 SCADAPack E outstation in the ClearSCADA database.

This method is the equivalent of updating the file properties via the Properties button on the Configuration Setup window (see Specify the Properties of a File in a SCADAPack E Outstation’s Configuration).

Arguments:


Disclaimer

ClearSCADA 2017 R3