Update a File in a SCADAPack E Outstation’s Configuration

Use the Update button on the Configuration Setup Window to replace an existing file with a more up-to-date copy of that file. This action allows you to retain the existing property settings for the file.

To update a file, select the file in the Configuration Setup window and then select Update. When you select the Update button, an Open window is displayed. Use the window to browse for the file with which you want to replace the selected file.

The specified file is only updated in the DNP3 SCADAPack E outstation’s configuration in ClearSCADA database when you select the OK button on the Configuration Setup window.

For further information, see Add a File to a SCADAPack E Outstation’s Configuration.


Disclaimer

ClearSCADA 2017 R3