Define the Historic Data Storage Properties

Use the fields within the Historic Data Filter section of the OPC tab to specify the type of data that ClearSCADA is to store historically for a Simple OPC analog point.

Use the Historic Data Filter section in conjunction with the settings on the Historic tab. The Historic tab settings define whether the server stores values historically for the point, and whether any unnecessary data is filtered out to reduce storage requirements (see Defining Historic Details for a Point in the ClearSCADA Guide to Core Point Configuration).

The ClearSCADA server retrieves and processes the current data values from the OPC server(s) that it monitors. Use the check boxes within the Historic Data Filter section to specify the type of retrieved data that ClearSCADA is to store historically for a particular analog point:

If neither of the check boxes above is selected, regardless of whether historic is enabled on the point’s Historic tab, ClearSCADA will not store retrieved point values historically.


Disclaimer

ClearSCADA 2017 R3