SCADAPack x70

Configure the Physical I/O Performance Properties

The SCADAPack x70 tab on the Forms of SCADAPack x70 Digital Configuration items contains a Physical I/O Performance section. Use the section to specify how the SCADAPack x70 device processes the point's data if the Digital Configuration item is associated with either of the following:

The Physical I/O Performance section contains these properties:


Disclaimer

ClearSCADA 2017 R3