SCADAPack x70

Configure the Properties on the Pulse Action Tab

The configuration Forms of SCADAPack x70 DNP3 Pulse Actions include a Pulse Action tab. Use the fields towards the top of the tab to configure these properties:

 

A Promote section is included at the bottom of the Pulse Action tab. Use the section to specify whether to promote retrieval of Pulse Control data (see Specify which Outstations are Integrity Polled after a Successful Control in the ClearSCADA Guide to the DNP3 Driver).


Disclaimer

ClearSCADA 2017 R3