SCADAPack x70

Create a Mimic to Display the Points

  1. Create a new Mimic.
  2. Drag-and-drop the SCADAPack x70 DNP3 Analog Output Point onto the Mimic.
    A context-sensitive menu is displayed.
  3. Select the Value option.
    A further menu is displayed.
  4. Select Formatted Value option.
  5. Drag-and-drop the SCADAPack x70 DNP3 Analog Input Point onto the Mimic.
    A context-sensitive menu is displayed.
  6. Select the Value option.
    A further menu is displayed.
  7. Select Formatted Value option.
  8. Save the Mimic.
  9. Put the Mimic into Run mode.

Once you have configured the Mimic, you can Download Configuration to the SCADAPack 575 Device.

Further Information

Working with Mimics: see the ClearSCADA Guide to Mimics.


Disclaimer

ClearSCADA 2017 R3