Description
Associated with: SCADAPack x70 Firmware Image items
This status attribute indicates the Description that was entered for the binary firmware image file when it was imported into the ClearSCADA database (see Import Firmware Image).
Use this status attribute in conjunction with the File attribute to ascertain information about the .biz file with which this particular Firmware Image item is associated.