SCADAPack x70

Downloaded Security Description

Associated with: SCADAPack x70 DNP3 Outstations that use DNP3 secure authentication.

This status attribute indicates the Description that was entered for the .rtk file when it was imported into the ClearSCADA database (see Import Security Configuration).

The attribute is only displayed if the Download Security Configuration pick action has been used to successfully download a security configuration file to the SCADAPack x70 device with which this SCADAPack x70 DNP3 Outstation database item is associated. The security configuration file comprises an .rtk file that has been imported into ClearSCADA.

Use this status attribute in conjunction with the Downloaded Security File status attribute to ascertain information about the .rtk file that was last downloaded to the SCADAPack x70 device.


Disclaimer

ClearSCADA 2017 R3