Minimum Configuration - Points
This topic relates to points on the SCADAPack x70 driver.
When you add an item to the database, various properties on the item's configuration Form are assigned a value automatically. These default values are assigned on creation of the database item, to help reduce the amount of manual configuration that is required. As such, you only need configure a subset of the properties that exist on an item's configuration Form. Typically, the properties you have to configure include:
- Those properties that require a value, but for which the property field is blank
- Those properties for which the value needs to differ from the default.
For a point on this driver to be capable of functioning in ClearSCADA, as a minimum you have to specify these properties on the point's configuration Form (the properties are on the <Point Type> tab unless stated otherwise):
- The protocol-specific SCADAPack x70 Outstation with which the point is associated
- The SCADAPack x70 Analog, Digital, or Counter Configuration item with which the point is associated
- If the point is an Analog Point, any additional Scaling that is required in ClearSCADA.
If the point is an output point, you have to:
-
Enable and configure the required properties on the Control tab.
If you want to store the point data historically, you have to:
- Enable and configure the properties on the Historic tab, to enable ClearSCADA to store the data historically in the server database.
- Enable and configure logging on the <Point Type> tab if data is to be stored historically at the outstation/controller.
Also ensure that the the database items on which the point depends are In Service, and have saved, valid configuration. This will produce a point that is capable of functioning using the default configuration settings.