SCADAPack x70

Specify the Scaling Applied by ClearSCADA

The Analog Point tab on the Forms of SCADAPack x70 DNP3 Analog Points contains a Scaling section. Use the section to define the scaling that ClearSCADA is to apply to the analog values that are reported by the SCADAPack x70 device.

The scaling that is applied in ClearSCADA is in addition to the scaling that is applied in the SCADAPack x70 device itself. The latter scaling is configured using the separate Scaling section on the Form of the SCADAPack x70 Analog Configuration item with which the Analog Point is associated (see Specify the SCADAPack x70 Device's Point Scaling)). The Analog Point inherits those Scaling settings from the Analog Configuration item - you can view the settings in the SCADAPack Scaling section of the Analog Point's Form.

You use the Multiplier and Offset fields within the Scaling section to define whether any additional scaling conversion is applied to the analog's values in ClearSCADA. For example, to convert values reported by the SCADAPack x70 device in Celsius into values in Fahrenheit for use in ClearSCADA.

The Scaling section contains these properties:

Further Information

Specify the SCADAPack x70 Device's Point Scaling.


Disclaimer

ClearSCADA 2017 R3