Configure a WITS Pulse (NULL) Action

Use the fields within the Actions section of the Pulse (NULL) tab to define the properties of the NULL pulse action. For more information, see Configure a NULL Pulse Action.

In the DNP3 WITS Driver, you can also set the following property for the NULL action:


Disclaimer

ClearSCADA 2017 R3