Dial In Device Port for a WITS Outstation

You can use the PSTN tab on the WITS Outstation Form to specify the Device Ports. For each dial-in line, specify the Field Device communication port for the modem (that is used to call ClearSCADA).

For more details, see Device Ports for WITS Field Devices.


Disclaimer

ClearSCADA 2017 R3