Export Program

Associated with: WITS Application Programs.

Security permission required to access this pick action: Configure.

You can use the Export Program action to export an application program file from ClearSCADA. The application program file can then be used in external applications.

When you select Export Program, a browse window is displayed - select a suitable location for the export file and enter a suitable filename. You should use the correct application program file syntax and include the version (see Application Program Files - Syntax and Transfer). Select OK to export the program.


Disclaimer

ClearSCADA 2017 R3