General Point Properties - WITS Mean Points

Use the fields at the top of the Mean tab to Configure General Point Properties.

The following field is specific to the WITS driver:


Disclaimer

ClearSCADA 2017 R3