Specify the WITS Properties

When configuring a WITS Field Device in ClearSCADA, you will need to use the settings on the WITS tab of the WITS Outstation Form (as well as settings on the other tabs of the Outstation Form).

WITS Outstation Form > WITS tab

The WITS tab contains settings that are specific to the WITS driver, including:

The Logged Data and Firmware settings on the WITS tab are only available if the features are supported by your Field Device (defined in its Device Profile, see Display a WITS Device Profile).

For information on displaying the Outstation Form, see Display a Form.

Further Information

How do I Configure ClearSCADA to Optimize the Use of the WITS-DNP3 Protocol?


Disclaimer

ClearSCADA 2017 R3