Trend Settings for WITS Integrator Points

You can display the trend, or movement, of the value of a WITS Integrator Point in the form of a graph.

The WITS Integrator Point is a type of analog point. Therefore, many of the fields in the Trend section of the Integrator tab are the same as those for other WITS analog points. However, an Integrator point trend is always linear, so there is no Logarithmic field (see Define an Analog Point's Trend Settings).


Disclaimer

ClearSCADA 2017 R3