Enable Alarms

If an item has its alarm features disabled and you want to re-enable them, you need to use the Enable Alarms action.

The Enable Alarms action can be triggered by a user, Logic program, Schedule or Method Call, but is only available if:

When the Enable Alarms action is used, alarms are no longer withheld for an item. This means that:

In the server configuration, there is an Independent setting in the Alarms section. This setting has an effect on how the Enable Alarms action is applied. In the following sections, we explain how Enable Alarms works when Independent is enabled and when Independent is disabled:

Before using the Enable Alarms action, we recommend that you familiarize yourself with the sections mentioned above.

NOTE: In addition to the pick actions mentioned here, ClearSCADA provides various methods that enable activities to be performed on alarms programmatically. This includes methods that are designed to trigger activities at specific times, such as the AcceptAtTime method that can be used to specify the time at which ClearSCADA is to acknowledge an alarm and to optionally log a comment for that acknowledgement. For more information on such methods, see the Database Schema (specifically the Methods section in the CAlarm class).


Disclaimer

ClearSCADA 2017 R3