Access the ODBC Data Source Administrator Tool

To set up ODBC Access, you need to use the ODBC Data Source Administrator Tool. The location of the ODBC Data Source Administrator Tool varies according to the Third Party application you are running and whether it is 32-bit or 64-bit. In the following sections, we explain how to access the ODBC Data Source Administrator.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3